Does the built-in excess temperature protection of the UPS pump need to be used?

If excess temperature protection is not properly connected or bridged, the pump may be permanently damaged. In addition, this will also void the pump's warranty.


    Facebook Twitter LinkedIn