Can the SP pumps also be operated in a horizontal position?

SP submersible pumps with a Grundfos or other submersible motor can be operated in any position from horizontal to vertical. The motor is arranged below the pump. A cooling jacket is generally required for these installation positions. See separate entry on this issue.

 


    Facebook Twitter LinkedIn